AnsweredAssumed Answered

STM32F103 Timer Interrupt Issue

Question asked by Praveen Gonsalves on Sep 7, 2017
Latest reply on May 1, 2018 by waclawek.jan

Hello, 

 

I'm using STM32F103RBT6 for my project, I've designed a custom board. 

I'm using cubemx to generate the basic code and Atollic for debugging.

I'm reading the switches using external interrupt. In the external interrupt call back, I'm starting a timer. 

In the timer interrupt handler, I'm doing some work. 

I've kept the timer timeout period to 2 seconds. 

My problem is whenever the code is started to run for the first time and when I press the switch, the code immediately  goes to the timer interrupt handler. This happens only once for the first time. After this, whenever I press the switch, code goes to the timer interrupt in 2 seconds which is correct. 

Why does it go immediately goes to the interrupt handler for the first time and then works fine thereafter??

I've attached the c file for reference. 

Is there any changes to be made??

Please suggest.

 

Regards

Praveen

Attachments

Outcomes