AnsweredAssumed Answered

Can I mask NRST signal input temporarily?

Question asked by tyro on Sep 5, 2017
Latest reply on Sep 6, 2017 by Clive One
Hi there,
I am coding STM32F030F4 using CubeMX generated EWARM project.
All ICs are monitored by single voltage supervisor including F030, but unfortunately one of IC has design problem and it need a "reset pulse" after start up.
I have to generate this reset pulse on F030 and the signal manipulates supervisor's manual reset input that reset also F030 itself.
So I would like to add NRST input mask routine for F030 while reset pulse sending operation.
Can I do this?
tyro

Outcomes