AnsweredAssumed Answered

STM32F469 add the USB driver to the Embedded Wizard Device Integration in uVison

Question asked by Daniel Wegen on Sep 5, 2017

Hello together,

 

i will describe my current status:

I use the STM32F469 Discovery Board and I have implementet the GUI from Embedded Wizard the Device Intergration Example and it runs in the example project from uVision.

 

I implementet the FreeRTOS direct from the STM32Cube_FW_F4 Library.

 

So I have the GUI + FreeRTOS + USART but I need the USB and thats my problem.

How can I simply add the USB to this project without long implementation time? If I would use the uVison CMSIS USB and FreeRTOS driver it shows some errors.

 

Is it possible to implement the USB from the STM32Cube_FW_F4 to my current FreeRTOS?

 

Is there anywere a manuel which includes from the USB I should do, without long searching and trying?

 

I hope you can help me, thanks for answers.

 

Best Regards,

 

DDMW

Outcomes