AnsweredAssumed Answered

I need 4 output with pwm feature. All pwm are the same period T of 200 Hz. All pwm have independent dc ( duty cycle ) and independent dt ( dead time ) . Is it possible configure the timer peripheral and the clock to have dead time configurable between 0 t

Question asked by giacomin.marco on Aug 31, 2017
Latest reply on Sep 6, 2017 by giacomin.marco
I need 4 output with pwm feature.
All pwm are the same period T of 200 Hz.
All pwm have independent dc ( duty cycle ) and independent dt ( dead time ) .
Is it possible configure the timer peripheral and the clock to have dead time configurable between 0 to T/2 ( half period )?
I'm using stm32f052 or stm32f072
thanks
Marco

Outcomes