AnsweredAssumed Answered

The lack of STM32 USART (interrupt mode) Example issue

Question asked by Carter Lee on Aug 30, 2017
Latest reply on Aug 30, 2017 by Clive One

Hi.
In order to implement STM32 USART (interrupt mode), so I've got STM32 USART (interrupt mode) Example file from here http://www.keil.com/download/docs/359.asp

 

But I've got a message from keil's uVision after build the project

 

"stm32f10x_map.h(30): error: #5: cannot open source input file "stm32f10x_conf.h": No such file or directory"

 

SO I've included relative file path into C/C++-> Include PATH


but still there is the lack of files.

So I want to get project file within sanity check.
How do I build up STM32 USART (interrupt mode) correctly? Can you help me to build up the example with STM32 USART (interrupt mode) Example ?

Attachments

Outcomes