AnsweredAssumed Answered

Abnormal operation after reset (BOOT0)

Question asked by Jae Bong on Aug 29, 2017
Latest reply on Aug 29, 2017 by David Siorpaes

STM32F103RC Abnormal symptom occurred while using Help request.

 

Resetting without a ground connection to the BOOT0 pin will result in some products not booting.

 

If this problem occurred from the beginning of development, it would have used to connect to ground. But I have been using it for 3 years now, it is frustrating because I have problems now.

 

Question 1: Why? Is there a product that boots after a reset, and a product that does not boot?

Question 2: Why? Is this problem only in recent products?

 

And I do not use the boot loader area

 

The problem is that the current BOOT0 pin can not be connected to ground

Outcomes