AnsweredAssumed Answered

Is there a listing of the program that come loaded on the STM32 Nucleo L031 board?

Question asked by Richard Cooke on Aug 28, 2017
Latest reply on Aug 29, 2017 by Richard Cooke

Hi Folks,

 

I've just started working with the STM32 NucleoL031 board and I think it would help me understand the system if I can find a listing of the program that is pre-loaded on the chip.  It blinks the green LED at one rate and if you put the jumper on that connects GND with D2 it will blink at a slower rate.

 

I've searched through the ST site but can't seem to find it.

 

Thanks in advance,

 

Richard

Outcomes