AnsweredAssumed Answered

Migrating a project to FW_F4_V1.16.0

Question asked by Ron Koch on Aug 24, 2017
Latest reply on Aug 24, 2017 by Clive One

I wanted to upgrade my F4 FW from 1.13 to the latest. For the STM32CubeMX Eclipse plugin to recognize the new FW I upgraded it to v.4.22.0 in the AC6 environment. I installed the F4 FW to v1.16.0 and migrated the project my project with the STM32CubeMX v4.22.0. I then updated my Project Properties paths to point to the new FW_F4_V1.16.0 location. 

 

I had some initial problems with errors in the HAL files that cleared up with reboots of the environment. But two problems persist. 

1) When I generate code in STM32CubeMX plugin I get the error window shown in the attachment.

 

2) When I try to build the project, I get errors in the HAL. Specifically, it can't find the declaration for the 'DMA_HandleTypeDef' structure in stm32f4xx_hal_dma.h even though this header is included. There may be more things that it can't find, but it bombs on this one. 

 

Any ideas? Thanks,

Attachments

Outcomes