AnsweredAssumed Answered

I am curious about the power consumption of the LSM6DS3.

Question asked by Seung-jin Lee on Aug 21, 2017
Latest reply on Sep 4, 2017 by Miroslav B

Hello.

I am curious about the power consumption of the LSM6DS3. 

 

The LSM6DS3 can set ODR independently.
However, the power consumption when the ODR is set independently is not listed in the Application note.
Only <Accelerometer only>, <Gyroscope only> and <Combo [Acc + Gyro]> are shown in Table 6.

 

I wonder how I can calculate it.
If the Accelerometer's ODR is set to 208Hz and the Gyroscope's ODR is set to 25Hz,

how much power does the sensor consume?

Outcomes