AnsweredAssumed Answered

X-NUCLEO-NFC03A1 problem with L152RET

Question asked by Nate River on Aug 20, 2017

Hi, I'm working on a project where I have to work with NFC protocol on my STM32L152RET.

I want to port to this board the nfc exemple coming with X-CUBE-NFC3 (it works as it should be with my F401RE).

I switched the HAL drivers for the L1xx HAL drivers.
When debugging I get stuck in an infinite loop interruption in the file startup_stm32l152xe.s :

 

"Default_Handler:

Infinite_Loop:

   b   Infinite_Loop"

 

The program cant get past the function ISO1443A_Init(); that ConfigManager_Taghunting is calling.

 

Can someone help me pointing out what is wrong ?

Outcomes