AnsweredAssumed Answered

STM32F7 USB library supporting multi-packet mode

Question asked by fortune.jean_pierre on Aug 15, 2017
Latest reply on Aug 24, 2017 by fortune.jean_pierre

Hi,

 

I need high USB bandwidth in isochronous mode. The STM32F7 is powerful but the bandwidth depends on how the USB packet management is done.

 

Is there a plan to support multi-packet mode in the HAL/lib/driver that come with STM32CubeMX?

 

The USB standard allows up to 3 packets per interval [3 x 1024 bytes every 125 μs in high speed].

 

This feature is supported in the "USB On-The-Go Host and Device Library", but it targets only F1/2/3/4 devices and is not easy to mix with CubeMX code.

 

An equivalent of DCD_EP_Tx, DCD_EP_PrepareRx, and so on. (with DMA support) in the LL layer produced by CubeMX would be ideal.

 

Thanks for your help.

Outcomes