AnsweredAssumed Answered

Suggestions for Non-Blocking I2C Slave

Question asked by horkin.charles on Aug 15, 2017

I'm using CubeMx with the STM32F415.

 

Looking at the HAL drivers for I2C slave devices using DMA, it appears as if the HAL_I2C_Slave_Receive_DMA() and HAL_I2C_Slave_Transmit_DMA() functions will effectively be blocking functions until the slave is addressed by a master ( There is a comment  /* Wait until ADDR flag is set */ ).  My code hangs there.

 

I want to implement a non-blocking receive function and a non-blocking transmit function.  It seems like the best way to do this would be to use the interrupts associated with the ADDRESS being acknowledged.  Has anyone done this?  Is there a better proposal?

 

Thanks.

Outcomes