AnsweredAssumed Answered

How to connect SMPS to control TRIAC with negative triggering circuit?

Question asked by Nazmul Hasan on Aug 14, 2017
Latest reply on Aug 14, 2017 by Nazmul Hasan

Hello

 

I want to control ST's snubberless triac (T435-800) directly from MCU (STM32F0). According to AN3168 (article 2.4), I've to connect AC main (220V, 50Hz) supply with the control circuit's Vdd. In AN392, I found the same that illustrate triac control with negative power supply, but uses capacitive dropper. Actually, I didn't understand what's going on there after connecting AC main with +5V DC. Why not the control circuit get affected by the AC main? All I want to do the same as AN392, but wants to use SMPS (STEVAL-ISA010V1, based on Viper16). Is it okay to connect SMPS's positive terminal directly to AC main? or Do I need anything else such as diode clipper?

 

Thanking you.

Outcomes