AnsweredAssumed Answered

SPI Clock bug in STM32CubeMX V4.3.1

Question asked by HarjitS on Sep 25, 2014
Latest reply on Sep 26, 2014 by Montassar BEN ROMDHANE
For the STM32F411, I set SPI 1 as a Full Duplex Master.

In the RCC Configuration, I set the VDD voltage to 3.3V.

In the SPI1 Configuration, I try to set the SPI Prescaler to /2 for a Baud Rate of 50.0 MBits/s, I get an error. According to the documentation, it should be fine.

STM32SPIBaudRateBug1of2.png

Clip from the datasheet:
STM32SPIBaudRateBug2of2.jpg

Attachments

Outcomes