AnsweredAssumed Answered

How to create USB Host using STM32F4 chip to communicate with USB Modems such as Telit?

Question asked by Daniel Hailu on Aug 10, 2017
Latest reply on Aug 15, 2017 by Lix Paulian

We need software written that implements a STM32F407 host mode USB driver, able to connect and communicate with USB serial devices that expose multiple virtual devices such as GSM/GPRS modems or Telit.

I wanted to get the drivers and library to use the STM32F chip as a host and connect to the Telit USB Modem.

* Implemented using this GCC toolchain 

* Using the standard STM32 USB base USB libraries

* Thread safe, implemented under FreeRTOS reference sample application

* Each discovered bi-directional stream presented as a stream from the library

Has someone done this before? If so can you help.

Outcomes