AnsweredAssumed Answered

SP5 Studio 5.5 Problem (CAN Issue)

Question asked by guo qiang on Aug 10, 2017

1.The CANConfig structure adds a number of field information,it have a "fifo_rx_callback" function point.

. Why is there a dialog box in SP5Studio that does not configure fifo_rx_callback?Causes the " fifo_rx_callback" function point to NULL

2. Building failed when disenable CAN filter.

this is a bug

Erwan YErwan Le RaySimon Scullion

Outcomes