AnsweredAssumed Answered

M24LR I2C pins driven low will RFID mode still work

Question asked by Andrew Lohmann on Aug 9, 2017
Latest reply on Aug 21, 2017 by NFC software support 3

My application will use NFC to either

  1. As a passive means of reading an identifier and to store or collect some simple information when a battery is discharged. In this case the I2C bus will be low. Also report that the battery condition.
  2. As a passive or powered means of doing the above plus pass information such as BlueTooth and Long range wireless keys transferred via IC2. Perhaps use NFC for some debugging as well.

I appreciate that I2C may need 10 clocks or something to recover from being in the wrong mode. That is fine.

 

  • My question is in (1) will the NFC operate correctly as a passive NFC device. That is with the I2C but pin held low during normal operation?

Outcomes