AnsweredAssumed Answered

L6470 problem: continuously read out status register

Question asked by ahlers.malte.001 on Dec 21, 2012
Latest reply on Dec 21, 2012 by ahlers.malte.001
Hi,

I’m playing around with the L6470 which finally worked quite well. But now I’m experiencing the following issue: I want to continuously monitor the status register of the L6470. But when I send a “run” command to the device immediately after using the “GetParam” command to read out the status register the motor does not move. If I do it the other way around i. e. when I first send the “run” command and then the “GetParam” command the motor turns as intended but I receive zeros (&H0) for the status register high and low byte. Have done something wrong or is it actually the case that there has to be a pause between sending two commands via SPI? If so, how long is this interval? And just to clarify: that would also mean, that there is a maximum frequency for changing the motor speed (e.g. it is not possible to send a new speed value at e.g. 1 kHz as needed for a quick control loop)?

I would very much appreciate any helpful hints. Thanks a lot!

Best,
Malte

Outcomes