AnsweredAssumed Answered

Problem with RTC

Question asked by Goran Overgaard on Aug 7, 2017

Hello

I have a problem that I can not solve.
This applies to stm32f072. I need to make a check if the processor has been powerless for more than 200ms at boot time. Trying to use RTC and backup registry with milliseconds.
In the main loop, I save the clock in the backup registry. And if there has been a voltage gap greater than 200 milliseconds, then errorflagga should be set. The problem is that whatever I do, then the clock reads from the shadow register. Have added
RTC-> ISR & = ~ RTC_ISR_RSF;
and RTC_BypassShadowCmd (ENABLE);
But this makes no difference.

Is there anything that knows how to solve this.

SIN Goran O

Outcomes