AnsweredAssumed Answered

drive the motor using STM32fr07vg

Question asked by m.vinothraj on Dec 20, 2012

Hi,
   i am trying to drive the motor using stm32f407vg. 
So i use the example code for this project from :
\STM32F4xx_DSP_StdPeriph_Lib_V1.0.1\Project\STM32F4xx_StdPeriph_Examples\TIM\6Steps.
i changed the code little.(from 6 channel from 4 channel).i am bit confused to use in timers and pwm.
but i could not get the desired result in oscilloscope  from my attempt . 
i want the result like attachment in this post.which example will i use? 
any suggestion...

Outcomes