AnsweredAssumed Answered

Copy example project does not work in System workbench

Question asked by sammalisto.pauli on Aug 3, 2017
Latest reply on Aug 9, 2017 by sammalisto.pauli

I am trying to import an example STemWin project to System workbench. I want to copy it, because I do not want to ruin the original one, I may need it for another project later, but if I check the copy alternative, only folders and names of the files are copied, and you maybe guess how it works. As I have learned, I am not alone with this problem in 2017. Pretty often (read always) I also get an Eclipse error, if I clean a CubeMx project and then I have to restart System workbench. I have W10.

 

Is this really the level of the STM framework today, late 2017?

 

The examples are less than one year old, but are not using HAL.  How long are these non-HAL libraries hanging around.

 

Where can I see the current workspace.  I can see previous workspaces, but where am I now.

Outcomes