AnsweredAssumed Answered

Wav player using DAC in STM32F429

Question asked by farouk majdoub on Jul 26, 2017
Latest reply on Feb 5, 2018 by Christopher Pappas

Hello,

 

I noticed that the stm32F429 disco does not have the CS43L22 circuit nor a 3.5mm jack for audio output as its rival the F407, but it has two internal DAC output, which can be used to play a wav file.

 

If anyone has an example compatible with HAL libraries would be very nice !

 

Farouk

Outcomes