AnsweredAssumed Answered

MOTENV1_ENABLE_PRINTF

Question asked by Dilbert K on Jul 26, 2017

HW : STM32L476RG-SensorTile

SW : SW4STM32

Tried to enable the debug print through USB.

I was using the BlueMicrosystem2_V2.2.0.  Enable  #define OSX_BMS_ENABLE_PRINTF and rebuild code will work.

Can see all the print out.

 

Recently got the new STM32CubeFunctionPack_MOTENV1_V3.0.0.

Followed the instruction in main.c to rebuild with #define  MOTENV1_ENABLE_PRINTF 

But the ST Virtual COM port not even showing up in PC device manager

 

Is there additional work need to be done ?

Outcomes