AnsweredAssumed Answered

STM Flash Loader support for STM32F423 CPU missing

Question asked by forest.jason on Jul 24, 2017
Latest reply on Jul 26, 2017 by STOne -32

Hello,

The current version 2.8.0, and the pre-release version V2.9.0RC4 floating around in the forum, do not support the STM32F423 CPU. There is no map file for this CPU. Is there an updated pre-release of the program that you can share with the support for this CPU?

 

Note: Even though we don't use the F413 CPU, it's in the same family as the F423, and support for this CPU is not present as well.

 

Thanks

Outcomes