AnsweredAssumed Answered

Differences between program with keil directly and stm32 st-link

Question asked by mohamadi.parisa on Jul 21, 2017
Latest reply on Jul 21, 2017 by Clive One

Hi,

I'm writing a code that works fine when I program directly via Keil with this settings

However if I compile the project and write hex file with stm32 st-link it doesn't work fine. It is good to mention that I active "read out protection" bit.

my means is that I my Ethernet protocol didn't work when I program with st-link however it works fine when I program it directly via keil with the same programmer.

Outcomes