AnsweredAssumed Answered

Bug when creating STM32L4 based projects using CubeMX

Question asked by Ant M on Jul 21, 2017
Latest reply on Oct 27, 2017 by Ant M

I am trying to create a project for either the L469 Discovery or Nucleo-144 board using CubeMX.

 

My setup is the following:

 

CubeMX 4.22.0

L4 Firmware v1.8.1

Using STM32 AC6 latest version

 

It appears as though CubeMX does not populate the FreeRTOS related directories with the required source files.

 

Doing the same thing for an F4 board I have no problem, so I'm assuming it is an issue specific to either cubeMX or the latest version of the L4 firmware.

 

Does anybody else have this issue?

 

Anthony. 

Outcomes