AnsweredAssumed Answered

stm32f103vbt6 Interrupt Numbers ?.

Question asked by Chris Quayle on Jul 20, 2017
Latest reply on Jul 21, 2017 by Clive One

Evaluating the above processor using gcc toolchain and openocd and J-Link. Not using cmsis (various reasons) and writing all the low level hal and header files, as a way to become more familiar with the processor. Already have  a simple non interrupt based program running, but need to understand the relationship between the interrupt numbers for the device and how these are derived. From what I can see, each device has a different set of interrupt numbers to control access to the nvic, but can find no docs that define that, after extensive web search and scan of the device data sheets etc. Would assume that this has been defined and docs must exist somewhere ?...

 

Regards,

Chris

Outcomes