AnsweredAssumed Answered

Problems found in STM32F746G-discovery Kit schematics

Question asked by NEERAJ GUPTA on Jul 19, 2017
Latest reply on Jul 20, 2017 by NEERAJ GUPTA

Refering to page no 6 in  mb1191.pdf  which is available as STM32F746G-discovery Kit schematic. 

The pin diagram of following two Arduino connector was incorrect, this need correction as follows:

1. CN4 connector has ARD_D5 pin mentioned as PA8 -> this is incorrect.

    ARD_D5 pin should be connected with PI0 as per rest of schematic.

2. CN7 connector has ARD_D10 pin mentioned as PI0 -> this is incorrect.

    ARD_D10 pin should be connected with PA8 as per rest of schematic.

 

Please! do this correction urgently. Otherwise it will create a lot of confusion regarding the hardware design.

 

Outcomes