AnsweredAssumed Answered

STM32Mx Cube features

Question asked by Balaraju Arror on Jul 13, 2017
Latest reply on Feb 8, 2018 by Jeanne Joly

Hello,

While using cube tool I got following questions. Can you please clarify them.

 

1. In general STM32Mx cube will generate drivers in the location where project file is there with folder structure  drivers/STM32F7xx_HAL_Driver/src.

Can we configure path to the generate driver files?

Can we configure the name of the generated folder in the tool?
2. In general STM32Mx cube will generate EWARM settings as well. This is not required on every change.

Can we generate only source files without settings?
3. We would like use EmbOS  as part of project. We need dynamic memory allocation for graphics . Does EmbOs support for the dynamic memory allocations? Do you have any idea on this point?

 

Thank you

Outcomes