AnsweredAssumed Answered

Is STM32 usable in this way?

Question asked by Hitoshi Ehira on Jul 13, 2017
Latest reply on Aug 7, 2017 by Tilen MAJERLE

Dear sirs,

 

I want to make drive recorder.

I think to use, USB(Mass drive), SD card small, TFT window ,camera(I want many cameras).

 

I do not want to make a proper product. I want only education or hobby.

 

I found two products.

1,STM32F4x7

2,STM32F469VIT6

 

1 is get pic slowly? (I need to 15fps or over) 

2 is employ both camera and TFT?

(I saw two function covered with a data sheet)

In addition, as for 2, are a camera and the LCD interface omitted with 100 pins and 144 pins?
thanks

Outcomes