AnsweredAssumed Answered

AppsNote for STM32CubeFunctionPack_MOTENV1

Question asked by Dilbert K on Jul 13, 2017

I just downloaded the new STM32CubeFunctionPack_MOTENV1_V3.0.0 and going through what motion sensor library could do all at once.

 

As I walk through the code in MEMSCallback(), all the W2ST_CHECK_HW_FEATURE checking is using "if" and not "else if"..... So is that meant all features can be detected all at once ?

For instance, can W2ST_HWF_FREE_FALL and W2ST_HWF_PEDOMETER  be enabled at the same time ?? and get correct status ?

 

Most specific to page 20 on "en.FP-SNS-MOTENV1_quick_start_guide", it shows all individual Motion features.

However, Mobile Apps would only able to show status one at a time.  Does, features actually running in parallel at firmware background ?

 

Any doc list out how Application was implemented ?

Outcomes