AnsweredAssumed Answered

LIS2DH FIFO in SPI mode

Question asked by David Kaplan on Jul 13, 2017
Latest reply on Sep 4, 2017 by Miroslav B

I did not quite understand from the pdf when reading 32*3 samples from the FIFO in SPI mode, can I set the SPI starting address at OUT_X_L (28h) with the SPI's MS bit raised and then read in a constant SPI read stream (single message) all of the 192 bytes?

 

Or do I need to read the SPI starting with  address (28h | 40h) in 32 different messages?

 

I saw in a previous post, that you can use the FIFO only in 10bit mode.

Is this true?

Outcomes