AnsweredAssumed Answered

Unterminated quoted string

Question asked by fff fff on Jul 13, 2017
Latest reply on Jul 13, 2017 by Clive One

Hi, i'm setting up Eclipse with GNU ARM Cross Compiler.

I made a simple Projekt ("blaccleds") with an STM32L0 Controller and the STM32L0xx_HAL_Driver-Package.

I get the following Console-Output with an Error Message when I try to compile:

 

16:43:00 **** Incremental Build of configuration Debug for project blaccleds ****
make all
Building target: blaccleds.elf
Invoking: GNU ARM Cross C++ Linker
arm-none-eabi-g++ -mcpu=cortex-m0 -mthumb -Og -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections -ffreestanding -fno-move-loop-invariants -Wall -Wextra -g3 -T mem.ld -T libs.ld -T sections.ld -nostartfiles -Xlinker --gc-sections -L"../ldscripts" -L"C:\STM32Cube_FW_L0_V1.9.0\Drivers\STM32L0xx_HAL_Driver\" -Wl,-Map,"blaccleds.map" --specs=nano.specs -o "blaccleds.elf" ./system/src/newlib/_cxx.o ./system/src/newlib/_exit.o ./system/src/newlib/_sbrk.o ./system/src/newlib/_startup.o ./system/src/newlib/_syscalls.o ./system/src/newlib/assert.o ./system/src/diag/Trace.o ./system/src/diag/trace_impl.o ./system/src/cortexm/_initialize_hardware.o ./system/src/cortexm/_reset_hardware.o ./system/src/cortexm/exception_handlers.o ./system/src/cmsis/system_DEVICE.o ./system/src/cmsis/vectors_DEVICE.o ./src/_write.o ./src/main.o ./src/stm32l0xx_hal_cortex.o ./src/stm32l0xx_hal_gpio.o ./src/stm32l0xx_ll_gpio.o
c:/gnutoolsarmembedded/buildtools/bin/bin/sh: syntax error: unterminated quoted string
make: *** [blaccleds.elf] Error 2
makefile:61: recipe for target 'blaccleds.elf' failed

16:43:00 Build Finished (took 228ms)

 

Can anybody tell me what's the Problem here?

Outcomes