AnsweredAssumed Answered

Debugging Skill and Pull Down Resistor

Question asked by j Q33 on Jul 11, 2017
Latest reply on Jul 13, 2017 by j Q33

Hi,

 

I have a quick question about the pull-up and the pull-down resistor.  For example, I want to use the switch (S1) to control the output of the GPIO pin (PA0), and read this output to turn on/off another LED.  When I set the GPIO pin,

   GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0;
   GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN;
   GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_DOWN;
   GPIO_Init(GPIOA, &GPIO_InitStructure);

I can make the program work as I expected when I set it to be pull-down or NOPULL (float?).  After some searching online, my understanding is that when I set the pin to have a pull-down resistor, there is a pull-down resistor shown in the figure, the PA0 is 0 when S1 is open and is 1 when S1 is closed.  Is my understanding correct?

 

 

 

 

Also, when I use the debug mode in Keil, there are a register block and a disassembly block shown on the screen but I do not know how to use them.  For example, I want to see the output of the pin PA0 in each step (when I press S1 or release S1), which part shall I look at?

 

Another minor question is that what will happen if I mistakenly set the mode to be pull-up.  Will the output always be HIGH, or somewhere randomly between HIGH and HIGH/2 (since I guess pull-up resistor and R64 divide the voltage by half)?

 

Thank you for your help!

Outcomes