AnsweredAssumed Answered

STM32L0 - USB Configuration

Question asked by Ciro Donnarumma on Jul 4, 2017

Hi,

 

I am writing a firmware for a USB device that uses the STM32L052K8 microcontroller.

Because my device must exhibit two USB interfaces, I have implemented a custom Composite Device class that acts like as broker: it dispatches the USB requests to the two standard USB classes on the basis of endpoint number or interface number present in the USB requests itself.

The first class is MSC- Bulk Only, therefore it has only two endpoints:

  • 0x81, a bluk input endpoint;
  • 0x01 a bulk output endpoint.

 The second class is custom class that has three endpoints:

  • 0x82, a bulk input endpoint;
  • 0x02, a bulk output endpoint;
  • 0x83, an interrupt input endpoint;

Except for 0x83, all of these endpoints have a maximum packet size of 64 bytes. The endpoint 0x83 has a maximum packet size of 8 bytes.

 

The problem is that the endpoints of the classes seems to interfere with each other, likely because I do something of wrong in the configuration of the USB peripheral PMA.

 

With the following configuration works only the MSC interface.

 

HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*) pdev->pData, 0x00, PCD_SNG_BUF, 0x18U + 0U * 0x40U);
HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*) pdev->pData, 0x80, PCD_SNG_BUF, 0x18U + 1U * 0x40U);
HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*) pdev->pData, 0x81, PCD_SNG_BUF, 0x18U + 2U * 0x40U);
HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*) pdev->pData, 0x01, PCD_SNG_BUF, 0x18U + 3U * 0x40U);
HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*) pdev->pData, 0x82, PCD_SNG_BUF, 0x18U + 4U * 0x40U);
HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*) pdev->pData, 0x02, PCD_SNG_BUF, 0x18U + 5U * 0x40U);
HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*) pdev->pData, 0x87, PCD_SNG_BUF, 0x18U + 6U * 0x40U);

 

Instead, if I change the endpoint index from 0x83 to 0x87 (everywhere, also in the descriptor), the situation seems better, but randomically  the device exhibits a wrong behaviour (the OS enumerates it two times and than it wokrs good).

 

Why do the behaviour  change if I chage only the endpoint index and not the endpoint address? 

Why the addresses in the PMA start from 0x18U?

What is the rule to evaluate the pma address?

Do I overwrite the BTABLE with the configuration above?

Is there something of wrong in the PMA configuration?

 

NB: When I changed the endpoint index, I also removed the device from Windows device manager. Furthermore this situation happened also on the NUCLEO-L053.

 

I'm sorry if my English is not perfect, 

Thank you very much

 

 

Outcomes