AnsweredAssumed Answered

How to change the program start address to the second section in an STM32F765VGT

Question asked by Rubén Acerete Halli on Jul 3, 2017
Latest reply on Jul 6, 2017 by Rubén Acerete Halli

Hello,

 

I need using the first 32Kb flash section in order to store data in an STM32F765VGT (1M of flash). How can I change the program start address to the second section. I’ve achieved to reallocate the program code in the second section by means of the linker script. But when I explore the first section with the stlink utility, in the first section, there is a piece of code instead of being empty. Furthermore if I erase this section the program stops working.

 

Thank you very much.

Outcomes