AnsweredAssumed Answered

Boost LED Driver

Question asked by shamsi.ammar on Jul 3, 2017
Latest reply on Jul 12, 2017 by shamsi.ammar
We are using LED6001 LED Driver in a Flasher.
The problem is when the input is less than 10.5V it works O.K but when the input is more than 10.5V the LED current reduces to almost 10mA or shuts down. The Problem is same with 6LEDs at the O/P and 12LEDs at the O/P. We have also tried shifting the OVP much above the O/P required volatage, but still this problem exists.
Please help us to resolve the problem.
 Please find the updated schematic.

Attachments

Outcomes