AnsweredAssumed Answered

VL53L0X measurement profile/spec

Question asked by herfurtner.alexander on Jun 30, 2017
Latest reply on Aug 15, 2017 by herfurtner.alexander

Hi,
changing the timing budget affects the measurment accurancy/speed/range.  This is done with the function VL53L0_SetMeasurementTimingBudgetMicroSeconds(..). Does this function affects the measurements parameter in the same way in case of CONTINUOUS_TIMED mode? So that I can take care about the timing budget (profile: long range, high acc.) and the internal time periode using the function VL53L0X_SetInterMeasurementPeriodMilliSeconds(...)?

 

Such like:
Timing Budget: 33 ms

Time Periode: 100 ms


With best regards

Alex

Outcomes