AnsweredAssumed Answered

STM32CubeMX hanging/not generating project on Mac

Question asked by Alexander Sparkowsky on Jun 27, 2017
Latest reply on Jun 27, 2017 by Alexander Sparkowsky

Hi,

 

I have an issue with generating the project code on any of my Macs running macOS. I'm using STM32CubeMX V4.21.0 but already discovered the same issue in previous versions.

 

Whenever I choose "Generate Code" from the "Project' menu CubeMX starts generating the project as expected.

The code generation stops at the stage "Generating XXX project..." (where XXX is any of the existing toolchains)  which means that the progress bar does not advance anymore and the generation is not completed. The application itself remains reactive.

I can quit CubeMX with the result of having an incomplete project without the toolchain specific project files (e.g. .project, Makefile, linker script etc.).

 

This problem is independent of the selected MCU and toolchain.

 

Can anybody help?

 

Alex

Outcomes