AnsweredAssumed Answered

STM32F051x programming system memory

Question asked by Daniel Manso on Jun 27, 2017
Latest reply on Jun 27, 2017 by Daniel Manso

hi everyone,

i´m working with the STM32F051.

I want to programm the System memory over the Serial interface using the ST Flash Loader Demonstrater.

So i set the BOOT0 Pin high, and connected the STM32F051 to the Computer.

Now i tried to use the ST Loader Demonstrater and i got the error message:

"This Version is not intended to suport the <STM32F0_63K> target".

The communication is possible when i´m using a terminal Programm and the Commands from the "AN3155".

Now my question:

is there any other way to programm the STM32F051 System Memory without sending single commands over an terminal programm?

Hope i made the problem clear.

I allready thank you for your help.

Outcomes