AnsweredAssumed Answered

Many problems with STM32-MAT

Question asked by corpa.enrique on Jun 23, 2017
Latest reply on May 16, 2018 by Johan Bloem

Hello,

 

I am having more or less the same kind of problems than the one in this post STM32_MAT/Target Error  I am trying a very simple program: a read IO block directly connected to a IO Write block. I started with Matlab R2015b, and after getting lots of errors I installed Matlab R2017a and now I am getting a different kind of errors, in particular this one: 

 

Attempt to call a non-function value: SLibModelInitFcnName

 

More details:

uVision 5.23

STM32CubeMx 4.21

STM32-MAT/TARGET 4.4.1

IOC file generated using the STM32F334 Nucleo discovery board setup, this is also the board that I have.

 

¿Is this really a problem related to my Matlab's version?¿Does a workaround exist?

 

I find this whole setup process very absurd and time consuming. ¿Does this really pay off when is up and running?

 

Here is the whole diagnostics prompt:

 

The "ARM CMSIS SIN COS" code replacement library includes the standard math library "C89/C90 (ANSI)". To avoid this warning, you can specify the code replacement library as "None" or remove the base CRL specification if applicable, then select the desired math library via the standard math library (TargetLangStandard) parameter. [2 similar]
### Real-Time Workshop build procedure for method: 'entry
### modelName: 'untitled
### gcs: 'untitled
### bdroot: 'untitled

### Starting Real-Time Workshop build procedure for model: untitled
### Windows version:win64
### Model connectivity is: normal
### Create verification block: None
Code Generation 2 1
Elapsed: 7 sec
### Generating code into build folder: C:\Users\Enrique\Desktop\Test\untitled_stm32
Source 'untitled/GPIO_Read' specifies that its sample time (-1) is back-inherited. You should explicitly specify the sample time of sources. You can disable this diagnostic by setting the 'Source block specifies -1 sample time' diagnostic to 'none' in the Sample Time group on the Diagnostics pane of the Configuration Parameters dialog box.
Component:Simulink | Category:Block warning
----------->STM32 MCU:stm32f3
### Real-Time Workshop build procedure for method: 'before_tlc
### modelName: 'untitled
### gcs: 'untitled
### bdroot: 'untitled
### before_tlc
### Invoking Target Language Compiler on untitled.rtw
### Using System Target File: C:\MATLAB\STM32-MAT\STM32\rtw\stm32.tlc
### Loading TLC function libraries
### Initial pass through model to cache user defined code
Warning: "---------->STM32_Config: MCU_Name is stm32f3"
.
### Caching model source code
Warning: simMode value is 0.0 0:RTW 1:PIL 2:EXT
Warning: Create real-time application main.c
Error: File: C:\Users\Enrique\Desktop\Test\untitled_stm32\tlc\customRoutineProcess.tlc Line: 359 Column: 27
Attempt to call a non-function value: SLibModelInitFcnName
Main program:
==> [00] C:\Users\Enrique\Desktop\Test\untitled_stm32\tlc\customRoutineProcess.tlc:<NONE>(359)
[01] C:\MATLAB\R2017a\rtw\c\tlc\mw\formatwide.tlc:<NONE>(483)
Error: File: C:\Users\Enrique\Desktop\Test\untitled_stm32\tlc\customRoutineProcess.tlc Line: 359 Column: 47
Values of NULL type cannot be expanded
Main program:
==> [00] C:\Users\Enrique\Desktop\Test\untitled_stm32\tlc\customRoutineProcess.tlc:<NONE>(359)
[01] C:\MATLAB\R2017a\rtw\c\tlc\mw\formatwide.tlc:<NONE>(483)
### Writing header file untitled.h
.
### Writing source file untitled.c
### Writing header file STM32_Config.h
### Writing header file untitled_types.h
### Writing header file rtwtypes.h
### Writing header file untitled_private.h
### Writing source file main.c
.
### TLC code generation complete.
### Real-Time Workshop build procedure for method: 'error
### modelName: 'untitled
### gcs: 'untitled
### bdroot: 'untitled
### Real-Time Workshop build procedure for model: 'untitled' aborted due to an error.
Error: Errors occurred - aborting

Outcomes