AnsweredAssumed Answered

Does STM32L-DISCOVERY and WITH Keil MDK Light V4.23

Question asked by b.c on Feb 18, 2012
I am able to open, compile and download both supplied projects from ST for the STM32L-DISCOVERY Framework. When running in DEBUG mode when the debugger excecutes the function Icc_run() at about line 221 in the AN3413 Current consumption.......... I get a STLinkIII error message "Internal command error" then "Error  attempting to read 64bytes  from 0x00000000"

Any help will be appreciated.

Outcomes