AnsweredAssumed Answered

[M24LR]Energy harvesting mode max current

Question asked by ostrysz.mateusz on Jun 19, 2017
Latest reply on Dec 20, 2017 by Jean-Louis Labyre

Hi,

I am working on wireless application and i would like to use energy harvesting mode of M24LR. I have a question about maximum harvested current. Datasheet is mentioning 6mA as the highest value. Is it possible to incrase this value by stronger magnetic field or bigger antenna (i need about 16mA)? Does the chip will handle bigger currents? Or maybe max range 6mA is only value above which energy harvesting output becomes active?

I would be grateful for any kind of help.

 

Best regards,

Mathew

Outcomes