AnsweredAssumed Answered

STM32F7 Disco ADC issue

Question asked by grozea.ion on Jun 13, 2017
Latest reply on Jun 13, 2017 by grozea.ion

Hello all,

I am trying to read the ADC value from PA0 pin on a STM32F7 Disco board but without any success.

The issue is that the ADC reading is acting as the pin is floating

I suspect that the initialization code is not correct due to the fact that if i change the the Pull parameter to PULLUP/DOWN the behavior of the ADC value stays the same.

I have try to run also the example ADC_RegularConversion_DMA from STM32Cube_FW_F7_V1.7.0 but the behavior of the value is the same (i run the code on 2 different new boards)

I have attached the ADC code for review.

Can someone help me figure it out what is wrong here?

Thanks

Attachments

Outcomes