AnsweredAssumed Answered

SPWF01S in MiniAP Mode with WEP Security

Question asked by Clara Antoine on Jun 12, 2017
Latest reply on Jun 12, 2017 by Gerardo Gallucci

Hello,

 

I configured my SPWF01S in miniAP Mode just like this:

 

# Dumping All Configuration Keys:
# nv_manuf = ST
# nv_model = SPWF01S
# nv_serial = value
# nv_wifi_macaddr = 00:80:E1:B8:6A:CC
# etf_mode = 0
# blink_led = 1
# wind_off_low = 0x00000000
# wind_off_medium = 0x00000000
# wind_off_high = 0x00000000
# user_desc = anonymous
# escape_seq = at+s.
# localecho1 = 0
# console1_speed = 115200
# console1_hwfc = 0
# console1_enabled = 1
# console1_delimiter = 0x0000002C
# console1_errs = 1
# sleep_enabled = 0
# standby_enabled = 0
# standby_time = 10
# wifi_tx_msdu_lifetime = 0
# wifi_rx_msdu_lifetime = 0
# wifi_operational_mode = 0x00000011
# wifi_beacon_wakeup = 1
# wifi_beacon_interval = 100
# wifi_listen_interval = 0
# wifi_rts_threshold = 3000
# wifi_ssid = 52:48:45:41:2D:54:49:54:41:4E:2D:4E:45:54:57:4F:52:4B:00:00:00:00:00:00:00:00:00:00:00:00:00:00
# wifi_ssid_len = 18
# wifi_txfail_thresh = 5
# wifi_ht_mode = 0
# wifi_channelnum = 6
# wifi_opr_rate_mask = 0x00003FCF
# wifi_bas_rate_mask = 0x0000000F
# wifi_mode = 3
# wifi_region = 1
# wifi_auth_type = 0
# wifi_atim_window = 0
# wifi_powersave = 0
# wifi_tx_power = 18
# wifi_rssi_thresh = 0
# wifi_rssi_hyst = 0
# wifi_ap_idle_timeout = 120
# wifi_beacon_loss_thresh = 10
# wifi_priv_mode = 1
# wifi_wep_keys[0] = 41:42:43:44:45:00:00:00:00:00:00:00:00:00:00:00
# wifi_wep_keys[1] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00
# wifi_wep_keys[2] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00
# wifi_wep_keys[3] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00
# wifi_wep_key_lens = 05:00:00:00
# wifi_wep_default_key = 0
# wifi_wpa_psk_raw = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00
# wifi_wpa_psk_text =
# ip_use_dhcp = 1
# ip_use_httpd = 1
# ip_mtu = 1500
# ip_hostname = iwm-B8-6A-CC
# ip_apdomainname = captiveportal.net
# ip_apredirect = firstset.html
# ip_ipaddr = 192.168.0.50
# ip_netmask = 255.255.255.0
# ip_gw = 192.168.0.1
# ip_dns = 192.168.0.1
# ip_http_get_recv_timeout = 3000
# ip_wait_timeout = 12000
# ip_dhcp_timeout = 20
# ip_sockd_timeout = 250
# ip_dhcp_lease_time = 120
# ip_dns_mode = 0
# ip_use_cgis = 0x0000000F
# ip_use_ssis = 0x0000000F
# ip_use_decoder = 0x00000000

 

I then try to connect an Android mobile phone to the AP. When I enter the wrong password, it is not working (hopefully). However when I enter the right password, it connects but I get this error:

 

+WIND:45:Dot11 AuthIllegal 25641/164

 

I saw that the first number should be a 0 or a 1.

 

Surprisingly, when connected I can exchange data through a socket between the 2 devices. So I don't understand where this error comes from..

 

Do you have any idea ?

 

Thanks,

 

Kind regards,

 

Clara

Outcomes