AnsweredAssumed Answered

Send LoRa packet with AT command - b-l072z-lrwan1

Question asked by Aaron Tsede on Jun 12, 2017
Latest reply on Aug 17, 2017 by Danny Chow

Hello,

 

I am trying to use LoRa connectivity with the brand new b-l072z-lrwan1 discovery board. The End Node project works perfectly but I have an issue with the AT Slave project. When I try to send LoRa packet to my Multitech gateway, this one never receive the packet and I cannot use AT command with the disco board anymore. I can only do a hardware reset of the board. 

As you can see on my screenshot, the Join process has been done correctly. After the AT+SEND command I never receive a status like OK or AT ERROR.

 

Are you able to help me ?

 

Thank you !

 

Aaron

Attachments

Outcomes