AnsweredAssumed Answered

SPWFxxxC with two antennas?

Question asked by Flow on Jun 12, 2017
Latest reply on Jun 13, 2017 by Gerardo Gallucci

Hi,

is it possible to use a splitter to have two wifi antennas with the SPWF moduls?

One antenna would be in side the housing, the second antenna shall have a cable with 1m length, e.g. http://www.teltonika.lt/de/product/wifi-antenna-5dbi-magnetic-type/ 

 

Using the modules u.fl connector and connect a cable with a SMA connector, then using a SMA splitter to connect the internal and the external antenna.

 

Are there any experiences about this?

 

BR,

Flow

Outcomes