AnsweredAssumed Answered

data ready interrupt lsm6dsl

Question asked by Geoffrey Raynal on Jun 9, 2017
Latest reply on Jun 12, 2017 by Miroslav B

Hello everyone,

 

I Would like read the lsm6dsl data by interrupt using the pin int1 on the sensor.

 

I configured the accelerometer ODR to 104 Hz

And i set up registers as follow :

 - Control_3C (0x12) =  64 (Data updated only when register has been readed / Interrupt level High / interrupt pin in push pull)

- Int1_CTRL (0x0d) = 1 (INT1_DRDY_XL enabled)

 

I get the first rising edge on int1 pin, this edge is detected by my MCU, I read status register and accelerometer datas but the int1 pin of the lsm6dsl stay in high level. How may I clear this interruption for the next set of data ?

 

Datasheet v :  DocID028475 Rev 6

 

Thanks

Geoffrey

Outcomes