AnsweredAssumed Answered

ST-LINK V2 Configuration Database

Question asked by David Instone on Jun 11, 2017
Latest reply on Jun 12, 2017 by David Instone

Hello all

I have an eBay ST-LINK V2 with an STM8S003F3P development board. Following the tutorial I have managed to get the project compiled without errors and set up the debugger options as instructed with the SWIM ST-LINK option. However when I attempt to start the debugger I get the Target Selection dialog which is fine but then the following error.

 

Starting debug session...
 -> Emulator reset (usb://usb)...
  ** Connection error (usb://usb): gdi-error [40201]: can't access configuration database

 

 -> Failed to connect target.

 

The tutorial did not mention I had to include the header file so is there a database that I am supposed to find. Anybody know where it is or what it is called?

Outcomes