AnsweredAssumed Answered

STM32F429I-DISC1 out of the box demonstration code not working?

Question asked by Pablo Leibovich on Jun 9, 2017

Hi everyone!

I've just bought an STM32F429I-DISC1 board. 

When I connect the board to the PC with the USB cable and all the jumpers as the manual said, the demonstration code starts and the screen with the image browser, video browser, game, calendar, performance and system info appears.

The problem is that when I connect an USB mass storage device to the USB User connector, the board doesn't recognize it.

It doesn't do anything with the USB, it's like if I haven't connected anything.

What can be happening?

Thanks!

Outcomes